This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906: Proper detection window size for PDF

Part Number: LMK04906

Hello support team,

There was a problem that the PLL did not lock on LMK04906.

After that, when PLL1_WND_SIZE (R24[2: 1]) is changed from 40 ns to 5.5 ns, it is now locked.

It seems that the setting was inappropriate because the detection window setting was 40 ns for PLL1_PDF of 40 MHz, but how much is the detection window suitable for PDF?

Best regards,
Kaizawa