Part Number: NE556
Other Parts Discussed in Thread: NE555
Attached is a circuit with 556 chip (i believe NE, SA, NA all should work). I have this circuit in a breadboard as well as on a PCB. The timer 1 should provide a one sot 8 second timer and timer 2 should provide a 0.5s ON and 0.5s OFF timer. The circuit as is where OUT1 is connected to RESET2 should provide a timer of 0.5s ON and 0.5s OFF for a total of 8 seconds INSTEAD i'm only getting a 1 seconds ON of LED and then it stays turned off. I checked this setup with 2 555's (connected their OUT to RESET as well) and individually tested the 2 timers inside 556, they work properly! when i connect them together, they just give an output of 1 second ON. Any thoughts?