This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00301: LMK00301 Additive Jitter at 2.5V VCCO

Part Number: LMK00301


Is the additive RMS Jitter Integration Bandwidth 1 MHz to 20 MHz for LVDS output, VCCO = 2.5V, and Clockin Frequency = 625 MHz available?  I can only find the additive jitter with VCCO = 3.3V for LVDS output on datasheet.