Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
I am using an external reference of 10 MHz. When I use TICs Pro sw I have no problem to get the proper signal (and the LD lock indicator is on), but when I want to program all the registers with the option "import hex file" I am not able to fix this value of f_osc to 10 MHz. I can change the N divider and fraction numerator and denominator, but the f_osc is still 100 MHz (I am copying the registers that appear when I set the f_osc value at 10 MHz but this registers only affect the fractional parameters). So, my question is, how can I set the local oscilator at 10 MHz through the registers?