Part Number: LMK01801
Hello,
We'd like to know if the LMK01801 clock input can be safely DC-coupled to a differential clock source? Nothing about CLKin input common-mode voltage can be found in the datasheet, and AC coupling seems to be the one and only recommended scheme.
Does anybody have details about CLKin equivalent circuit?
On evaluation board we measured around 1.8V at the CLKin pins. So it seems that for instance 3.3V LVPECL driver format (VCM usually VCC-1.4V) could fit well to roughly match CLKin common-mode voltage level. Is this assumption correct?
Best regards,
Joerg