Part Number: LMK03318
Other Parts Discussed in Thread: CDCE913
I'm looking for a low jitter clock generator to generate multiple clocks ranging from 200kHz to 300MHz using a 30.72MHz input clock. Noticed that the data sheet for the above part specifies a 40 - 60% duty cycle for the input clock.
However, my 30.72MHz input clock has a 35% duty cycle. Just wondering what is dictating the 40 - 60% duty cycle and if the LMK03318 will work with 30.72MHz input clock at 35% duty cycle. If not then would be grateful if you could suggest alternative solutions.
Many thanks