Part Number: LMX2492EVM
Other Parts Discussed in Thread: LMX2594, LMX2492,
I was measuring the power of RF_out port a 10.5GHz and found that the output power is at the level of approximately -5dBm. According to the datasheet of the VCO, the minimum output power at the RF port is +4dBm and a typical output power at +7dBm. With a resistive power divider on the evaluation board, I assumed that the power at RF_out port should be approximately -2dBm(i.e. +4dBm - 6dB), but I got -5dBm. I am trying to find out where is the extra losses coming from. How good is the resistors used in the divider at 10GHz?
I crossed checked the EVM manual where the RF_out/2 port was measured and the frequency was 4.8GHz. There is no power divider on the board for the RF_out/2 port and the output power from the VCO chip should be +1dBm(min) and +4dBm(typ). Figure 6 in the manual shows that the power is -3.15dBm. Again, why is the measured output power much lower than the level specified in the VCO chip datasheet?