Hello,
I want to connect the DELAY/M_DRV pin directly to a micro controller output to assert the DRVN pin. Is it possible ? It is not clear in the datasheet. In section 6.5 it mentions that LOGIC_HIGH on M_DRV pin is anything above 1.5V, however in section 7.5.2 it says VDD must be applied on DEALY/M_DRV pin to recognize as manual Power ON.
Please clarify.
Thanks..... Pradeep