This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I develop board with 10 x DAC5682Z & 2 x ADS5400.
I looking for clocking solution, I saw LMK04816/28 but it will be great if you can suggest your recommendation.
Skew need to be lowest as possible, does the skew are for 2 close outputs (for example out0 & out 1) or for 2 extreme outputs (for example out0 & out11)?
Jitter lowest than 1psec.
Freq of 1GHz
For ADS5400 the clock and the trigger need to come together.
If you think about different solution than the attached diagram please offer.
Thanks,
Shlomi