Part Number: LMX2572
Other Parts Discussed in Thread: LMX2594, LMX2595
I have problems with output power at RFOutAP. RFOutAM is symmetrically terminated into a 50 Ohm resistor and OutB powered down.
My goal was to implement a step by step ramp in full assist mode, since I couldn't get the manual ramp to lock quick enough. This ought to go from 4 GHz to 6 GHz, so OUTA_MUX = 1 (direct VCO output).
When I sweep through from 1.6 GHz to 6.4 GHz I get decent power from the channel divider output, but when the MUX out is switched to VCO the output power almost vanishes.
Similar ramps work on LMX2594 and also LMX2595.
I removed pull up reistors at output of the 2572 and almost tried every setting for OUTA_PWR.
Do you have any idea?