In above thread, I heard that a pulling range of CDCE913 can be calculated by following expression.
Pullability (ppm/pF) = C1 * 1e6 / [2 * (C0 + CL)^2 ]
Pulling Range (ppm) = Pullability * CL
So, I selected a below crystal.
CL: 8 pF
C0: 1.3 pF
C1: 5.08 fF
-> Pullability = 29.4 (ppm/pF)
Pulling Range = 235 (ppm)
Then I replaced the crystal on our board with it, and I measured pulling range.
(How I measured it is described in above thread.)
As a result, the pulling range of it was 133ppm.
It is quite a bit different from the calculated value.
[1st question]
I think that "parasitic board capacitance" might affect the result mainly.
Is this thought correct?
If there are any other factor affecting the result, please tell me.
[2nd question]
If it affects the result, where should the value of it be inserted in the above expression?
ex) Pullability (ppm/pF) = C1 * 1e6 / [2 * (C0 + CL + Cpar)^2 ]
(Cpar: parasitic board capacitance)
[3rd question]
Why the displayed unit of "Crystal" in "Pulling Range Plot" of "TI Clock Pro" is "fF" ?
In above thread, I heard that the "Crystal" means "Load Capacitance" of a target crystal.
If so, I think that the unit should be "pF".
Best Regards