Part Number: LMX2541
Other Parts Discussed in Thread: LMX2571, , LMX2572, LMX2485, LMX2491
I went through the data sheet, but I am not clear on the power consumption of the device. I plan to use the device in the external VCO mode with divider ratio up to 8.
1. The data sheet page 7 shows the current consumption. Ipll=72mA and Idiv=84mA. Why Ipll is lower current than Idiv? The divider only mode should turn off the PLL, so Ipll should be higher than Idiv.
2. Page 35 Table 17 shows Change is current consumption in div mode as a function of DIVGAIN and OUTTERM, and the reference is when each parameter set to 12. but because of above question, I can't set the absolute current as the reference.
3. Does Idiv vary depending on the divider ratio?
What I want to know is that the actual (approximate) current under these conditions:
Mode: external VCO
External VCO frequency: 1000MHz ~ 2000MHz
PD frequency: ~ 4.8MHz
Divider: ~ 8
DIVGAIN and OUTTERM: 12
Thank you