Part Number: LMX2594
Hi,
I am using the following setting for check PLL lock detect:
MUXOUT_LD_SEL = Lock Detect
LD_TYPE = Vtune and VCOCal
It seems to work well when I was testing it for a fixed frequency where the signal when low (indicating 'Cal') to high (indicating 'locked'). However this is not the case when I am using running an automatic ramp. The signal seems to stay low all the time.
I would like to have a 'flag' out from the PLL to indicate the automatic ramp is started after writing the RAMP_EN bit. Is it possible with LMX2594?
Thanks.