This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: Best setting to use for a jitter cleaner audio application

Part Number: LMK03318

Hi,

I am using the LMK03318 as a jitter cleaner for an Audio clock source that requires a jitter of <5ps. I am converting an MCLK of 24.576MHz to an audio sample clock of 12.288MHz. I have included a plot of the jitter characteristics of the MCLK. Would you be able to recommended the best setting for this application.

Thanks

Regards

Billmclk_jitter_statistics_181201_000.pdf

  • Hi Bill,

    The attached file contains the register settings configured for your use case. Use these settings as a starting point if you need to further optimize the configuration.

    Kind regards,
    Lane

  • Hi Lane,

    Thanks for the response. Did you attach a file?

    Regards
    Bill
  • As far as I can tell the file was not attached?
  • Hi Bill,

    My apologies. Please see attached.

    Kind regards,
    Lane

    R0	0x0010
    R1	0x010B
    R2	0x0233
    R3	0x0301
    R4	0x0401
    R5	0x0500
    R6	0x0636
    R7	0x07DC
    R8	0x0822
    R9	0x0900
    R10	0x0AA8
    R11	0x0B02
    R12	0x0CD9
    R13	0x0D00
    R14	0x0E1D
    R15	0x0F00
    R16	0x1000
    R17	0x1100
    R18	0x1200
    R19	0x1300
    R20	0x14FF
    R21	0x15FF
    R22	0x16FF
    R23	0x1703
    R24	0x1800
    R25	0x19F5
    R27	0x1B20
    R28	0x1C00
    R29	0x1D02
    R30	0x1E3B
    R31	0x1F30
    R32	0x2030
    R33	0x21C3
    R34	0x2230
    R35	0x2330
    R36	0x24C3
    R37	0x253E
    R38	0x26C3
    R39	0x2718
    R40	0x28C3
    R41	0x2918
    R42	0x2AC3
    R43	0x2B18
    R44	0x2CC3
    R45	0x2D0F
    R46	0x2E00
    R49	0x310A
    R50	0x3285
    R51	0x3303
    R52	0x3400
    R53	0x3500
    R56	0x3802
    R57	0x3918
    R58	0x3A00
    R59	0x3B62
    R60	0x3C00
    R61	0x3D00
    R62	0x3E00
    R63	0x3F00
    R64	0x4000
    R65	0x4101
    R66	0x420C
    R67	0x4308
    R68	0x4401
    R69	0x4504
    R70	0x4607
    R71	0x471F
    R72	0x4818
    R86	0x5600
    R88	0x5800
    R89	0x59DE
    R90	0x5A01
    R91	0x5B18
    R92	0x5C01
    R93	0x5D4B
    R94	0x5E01
    R95	0x5F86
    R96	0x6001
    R97	0x61BE
    R98	0x6201
    R99	0x63FE
    R100	0x6402
    R101	0x6547
    R102	0x6602
    R103	0x679E
    R104	0x6800
    R105	0x6900
    R106	0x6A05
    R107	0x6B0F
    R108	0x6C0F
    R109	0x6D0F
    R110	0x6E0F
    R115	0x7308
    R116	0x7419
    R117	0x7500
    R118	0x7607
    R119	0x7701
    R120	0x7800
    R121	0x790F
    R122	0x7A0F
    R123	0x7B0F
    R124	0x7C0F
    R129	0x8108
    R130	0x8219
    R132	0x8403
    R135	0x8738
    R136	0x882B
    R137	0x8910
    R138	0x8A38
    R139	0x8B00
    R140	0x8C00
    R141	0x8D2B
    R142	0x8EFF
    R143	0x8F00
    R144	0x9000
    R145	0x9100
    R169	0xA940
    R172	0xAC24
    R173	0xAD00
    

  • Hi Lane,

    I have tried these setting and I am not getting anything out of channel 4. I did a register read back after writing the values to the LMK03318. The spreadsheet contains the values written and the values readback.

    I did notice that registers R5, R6, R7, R169, R172 and R173 are loaded with values but these registers are not defined in the datasheet.

    Any ideas on why there is no output?

    Thanks

    Regards

    Bill

    lmk03318_register_setup_181205_000.xlsx

  • lmk03318_almost_locking_waveform_181205_000.pdfHi Lane,

    I have included a plot of the waveforms. It looks like the output on channel 4 occurs after the VCO calibration cycle but the LMK looses lock shortly afterwards. 

    Yellow: PRIREF_P

    Pink: OUT4_p

    Blue: STATUS0 - PLL VCO Calibration Active (CAL)

    Green: STATUS1 - PLL Loss of Lock (LOL)

    Regards

    Bill

  • Hi Lane,

    I have been able to get the PLL to lock. To get the PLL to lock I changed how the input clock to PRIREF_P was being generated.

    I would like to use STATUS0 as the output of the PLL clock. I have programmed the following on top of existing values you recommended but do not see any output from STATUS0. Would you be able to advise on setting STATUS0 as the output of the PLL clock?

    Regards

    Bill

    0x1E=0x3B // R30

    0x2D=0x18  // R45 Set STATUS0 as a clock output with /4

    0x2E= 0x61 // R46 Set STATUS0 integer divide value 98 (4816896000/(4*98)=12.288MHz

    lmk03318_locking_waveform_181210_000.pdf

    4816896000
  • Hi Lane,

    I have been able to get the PLL to lock. To get the PLL to lock I changed how the input clock to PRIREF_P was being generated.

    I would like to use STATUS0 as the output of the PLL clock. I have programmed the following on top of existing values you recommended but do not see any output from STATUS0. Would you be able to advise on setting STATUS0 as the output of the PLL clock?

    Regards

    Bill

    0x1E=0x3B // R30

    0x2D=0x18 // R45 Set STATUS0 as a clock output with /4

    0x2E= 0x61 // R46 Set STATUS0 integer divide value 98 (4816896000/(4*98)=12.288MHz
  • Hi Bill,

    I set 0x2D = 0x1C to disable STATUS1 and enable the STATUS0 CMOS clock

    Kind regards,
    Lane
  • Hi Lane,

    I have tried both 0x2D=0x1C and 0x2D=0x18. Both setting should result in a clock signal out of STATUS0. Neither one is working with my setup. I have included a complete list of my register writes and also the readback values.

    Any ideas on why there would be no output from STATUS0?

    Regards

    Bill

    register_writes_181211_000.xlsx

  • Hi Lane,

    I have tried both 0x2D=0x1C and 0x2D=0x18. Both setting should result in a clock signal out of STATUS0. Neither one is working with my setup. I have included a complete list of my register writes and also the readback values.

    Any ideas on why there would be no output from STATUS0?

    Regards

    Bill
  • Hi Bill,

    I converted your register setting into TICs Pro configuration. Didn't find any problem.

    Could you use reset bit (R12.bit 7) again to see what happened?

    LMK03318 TICS Pro configuration.zip

    Best Regards,

    Shawn

  • Hi Bill,

    Sorry for the delay. As Shawn mentioned, you may need to toggle the reset bit in order to re-calibrate the PLL if the outputs are not present.

    One thing that may help with your debug is setting the STATUS1 output to PLL LOL in order to determine whether the PLL is locked.

    Kind regards,
    Lane