This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: Output clock frequency is incorrect / wrong settings?

Part Number: CDCI6214

Hi TI-Team,

I am trying to get 270 MHz out of a CDCI6214.

I have used the TICS Pro to get the settings for that. After running the wizard I get the following configuration:

However with this configuration I am getting ~232MHz at all the output ports.

We are using a 27MHz LVCMOS clock as input reference which is clean.

Do you have any idea what we are doing wrong?

Thank you very much

BR

Tobias