Part Number: LMX2492EVM
Other Parts Discussed in Thread: USB2ANY, LMX2595EVM
Dear Noel,
The LMX2492EVM wirh USB2ANY was working fine, until I used a USB cable of 10 meters, the USB interface connection did not work stable anymore.
The TIC Pro was asking for a Firmware update, (probably due to the poor data tranfer over 10 m.) the update failed.
since then the USB2ANY is not detetcted by the TICS Pro.
See figure 28 and 29 of the SNAU160E, The information on Figure 29 was:"Firmware not correctly loaded and the system halted here.
Question, How can reload the firmware in the USB2ANY, or how can I come into figure 25 of SNA160E to reload firmware?
In the mean time I use a Reference-Pro USB interface (of the LMX2595EVM) for the LMX2492EVM,
Looking forward to a solution.
Kind Regards,
Bert