Other Parts Discussed in Thread: TLC555
Hi
We are having some issue matching calculated and real (tested) frequency output with LMC555 in 50% Duty Cycle Oscillator mode.
The formula for frequency calculation is: f = 1/(1.4 * Rc * C) [page 16 in the datasheet: LMC555 SNAS558M –FEBRUARY 2000–REVISED JULY 2016 ]
We used these components:
Rc = 4.7 MOhm; C = 1.8 pF
f = 1/(1.4 * 4.7e+6 * 1.8e-12) = 84,431 Hz
f (tested) = 22,500 Hz
However, with other components:
Rc = 8 KOhm; C = 1070 pF;
f = 1/(1.4 * 8E+3 * 1.07E-09) = 83,445 Hz
f (tested) = 84,200 Hz
Any idea what could be wrong?