This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVD2102: Is the CDCLVD2102 recommended/suitable for driving LVDS over a long backplane?

Part Number: CDCLVD2102


Hi, 

I understand from the datasheet that the CDCLVD2102 is suitable for driving 100 ohm differential loads with its differential LVDS outputs. I would like to know if TI considers this part suitable to drive LVDS pairs over a long backplane (perhaps on the order of 15 inches) or would recommend it for such a purpose. 

Thanks