This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE72010: SPI Interface

Part Number: CDCE72010

Hello

Do you Possible the SPI Configuration when Reset or Hold Mode?(Use Pin #33)

Regards

  • If I understand your question correctly, you would like to know if it is possible to program the CDCE72010 via SPI when the device is in RESET or HOLD mode?

    Based on my understanding of the datasheet, it appears that the device can be configured by SPI while in RESET or HOLD mode. However, the datasheet does not clearly state whether it is possible or not.

    By default, Pin #33 is configured as a RESET input.

    I hope this information helps.

    Kind regards,
    Lane