Other Parts Discussed in Thread: CDCE62002, CDCE62005
Hello,
I'm looking for a clock synthesizer capable of generating any frequency from a primary and a secondary input clock sources.
Basically, I need to generate 292MHz and 147 MHz from a 10 MHz primary clock reference. If the primary reference disappears, the reference is switched (hitless) to the secondary clock input which would be a high precison TCXO. (like operates Si5326 from silicon Labs in Free Run mode).
Would the cdce62002 be a good choice?Any better option? Is there an any-frequency clock generator from TI which allows automatic switching reference?
Thanks.