Part Number: CDCM7005
Other Parts Discussed in Thread: ADC16DV160,
HI
I want to connect both a DAC (DAC5682) and an ADC (ADC16DV160) to an FPGA board (NEXYS VIDEO) via an FMC connector. I have a very limited amount of pins, so I have decided to use the CDCM7005 to generate the various clock signals from 1 signal. I have gone through the datasheet but there are Things i am not sure about.
I want to use the CDCM7005 to generate a 320 MHz and a 160 MHz clock signal.
One option is to send 1 clock signal at 320 MHz from the FPGA.
Another option is to generate the 320 MHz clock signal from a VCXO.
In both cases I also generate a clock signal to go back to the FPGA for synchronisation with the DAC and ADC.
Im an not set on the frequency, I might want to sample slower.
My question regards the reference clock (PRI_REF, SEC_REF)
If i look at the example in the datasheet 10.1.1 it seems like the reference clock is 128 times smaller than the input clock, is that a general factor or how is the value 3.84 MHz determined?
Another question is wether the reference clock is nessassary or not.
Do I only need the reference clock if I use the PLL-mode? Do I need it if the 320 MHz clock is generated from the VCXO, or do I need it in general?
Regards
Michelle