Other Parts Discussed in Thread: CDCE62005
Hi,
I'm using the CDCE62005 clock synthesiser on my board. I'm hooking up the decoupling based on the CDCE62005 evaluation card schematic. However there's a connection to VCCA on Page 13 of the document. VCCA is also mentioned in the datasheet within the Analog Supplies. However, I'm not sure what to connect this to, or what pins to put the two 0.1uF caps next to. I reckon I've got all the other caps going to or near a pin. So what should VCCA connect to and where should these caps be placed?
Thanks
Stuart