Part Number: CDCLVP1102
Other Parts Discussed in Thread: LMK03806, LMK04133
Hi,
I have a image sensor which requires a differential clock of 400Mhz
the clock to the sensor comes from a different fpga board which is connected through a 5 inch flex cable
so i want to use a clock buffer CDCLVP1102 before sensor clock input as the high speed clock coming through connector may become jittered
kindly help in how to connect LVDS clock through this buffer, is this a right choice, is there any low power variant of same ?
1. can make VCC 3.3v ? or it should 2.5 V ?
2. what to do with AC_REF pin ? can i just leave it unconnected as its only required for LVPECL
3. should i have to put a 100 ohm termination at both input and output of CDCLVP1102 ?
4. there are two output for buffer can i ignore the other (OUTP[1] and OUTN[1]) which are unused ?