Part Number: LMX2595
Hello guys,
I have one issue with the LMX2595 chip.
I am getting a strong 50Hz spur along with the generated frequency. It is 40 dB down.
Are there any particular ways to filter it out in both hardware or software...
I am using a 230V 50 Hz AC mains to feed a lab DC power supply from which I am feeding +5V to a low noise regulator.. which generates +3.3V required for the chip.
The same card generates the voltages for the OCXO being used using a low noise regulator.
Please suggest where could be the possible problems.
The