Part Number: LMK04610
Other Parts Discussed in Thread: LMK04616EVM, LMK04616, LMK04828, LMK04832
Hi, Team
My customer is using LMK04610, and they would like to keep the output clock has fixed phase delay than input clock.
This can be set by the zero delay mode by use feedback as Ouput Clock 7/8 descripted in datasheet.
But we found that once temperature is changing, for example from -40 to 25 ℃, the output clock phase will shift a lot.
I tried to reduplicated this in a LMK04616EVM which is the same problem.
Can you please help to check if this is expected or any way to optimize it to very little phase shift?
I've captured a video. CH1 is input CLKIN1, CH2 is OUTPUT9 which is same frequency as input of 122.88MHz.
Firstly I loaded the default setting from TICS, then I change it to the zero delay mode by setting feedback as OUTPUT 7(983.04MHz). It will locked well.
Then I will use freeze spray to cool down the LMK04616 on the EVM. The CH2 will shifting as video showed.