This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: EEPROM mapping of the register only defined the register map

Part Number: LMK03328

Hi,

Below register is defined only register map in datasheet.

Could you let me know address on EEPROM, please?

- PARTID[7:0]

- STATCTL[3:2]

- IPCLKCTL[6:3]

- PLL1_LF_R3[0]

- PLL2_LF_R3[0]

 

Best regards,

Kenji

  • Hi Kenji,

    - PARTID[7:0] : PARTID Register; R4 , Each LMK03328 device can be identified by a unique 8-bit number stored in the PARTID register. This register is

    always initialized from on-chip EEPROM. This value is reserved. It is better not to modify it. You can find the address in EEPROM  by TICS Pro as below figure.

    - STATCTL[3:2]: reserved. Do not change them.

    - IPCLKCTL[6:3]: reserved

    - PLL1_LF_R3[0] &,- PLL2_LF_R3[0]: Located in Byte 71[4] &  BYte 82[2]

    Noticed total 7 bits saved in EEPROM for each PLLx_LF_R3 register.

    Regards,

    Shawn