Part Number: LMX2491
Hi Sir,
Currently use STM32F401 to setup TI LMX2491, the Frequency is 24.15GHz, we would like to know whether there has any related reference Sample code or how to control it for the specific scheme.
Ja
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2491
Hi Sir,
Currently use STM32F401 to setup TI LMX2491, the Frequency is 24.15GHz, we would like to know whether there has any related reference Sample code or how to control it for the specific scheme.
Ja
Hi
We still have issue about how to ensure that the corresponding output of the SPI command is correct. We have done the following action, but still not work.
1. We created register values by TICS pro and send them via SPI interface. But when we measured the CPout, it showed about 400mV
2. We use the logic analyzer to measure spi can go out from muc, and the signal is the same as what I sent.
3. In addition, I also have a test to set the register of 0x02, but still the same, cpout is 400mV
4. In addition, this is a separate test of Power on code.
uint8_t Lmx2491_PowerOn(void)
{
TransDoneFlag = 0;
uint16_t j, k;
uint8_t aTxBufferTemp[] = {0x00, 0x02, 0x01};
Lmx2491_LE_L(); //Start transfer, pull down LE
for(k = 0; k < 20000; k++){}
for(k = 0; k < 20000; k++){}
for(k = 0; k < 20000; k++){}
HAL_SPI_Transmit_DMA(&hspi2, (uint8_t*)aTxBufferTemp, (sizeof(aTxBufferTemp)));
for(j = 0; j < SPI_TIMOUT; j++)
{
for(k = 0; k < 20000; k++){}
if(TransDoneFlag == 1)
{
break;
}
}
ResetTxDoneFlag();
//Error or Finish, pull up LE
Lmx2491_LE_H();
if(j >= SPI_TIMOUT)
{
return 0;
}
return 1;
}
5. TICS_Pro_Configer.tcs, please check attached file.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/48/TICS_5F00_Pro_5F00_Configer.7z
Hi
Sorry, we do not have EVM. Please help to suggest alternative way. Thanks.