This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCVF2310: Is that device 3.3v tolerant when it is powered by 2.5v ?

Part Number: CDCVF2310


In its Datasheet under the recommended operating conditions no maximum value is written for the Vih under VDD=2.3 to 2.7 V.

Is that mean, that 3.3v or any other voltage smaller than the Absolute Maximum Rating limit is tolerant in the clk input ?