Part Number: LMK04832
Tool/software: WEBENCH® Design Tools
Hi
I want to re-design the loop filter for LMK04832 for both PLLs. However the webbench tools doesnot support it. I tried using platinum tool, with the same user guide values from LMK04832, it shows different loop filters results.
Here are the Inputs, For PLL1, Input frequency 10MHz, fpd =1MHz, Loop BW = 14Hz, Phase margin = 50, Kpd = 0.45mA, Kvco = 2.5KHz/V, Output freq = 100MHz, VCXO =100MHz.
For PLL2, Input frequency = 100MHz, Fpd = 100MHz, Loop BW = 220KHz, Phase margin =70, Kpd = 3.2mA, Kvco = 13.6MHz/V, Output freq, 10MHz, 100MHz, 50MHz. So I am using VCO0.
I am optimizing for Lowest possible Jitter. Can you provide me the optimal loop filter settings and values ?
Regards
Venu