Part Number: CDCLVD1204
Other Parts Discussed in Thread: CDCLVD1213
Section 11.3 describes a current draw of 186mA and a supply voltage of 3.6V, 669.6mW
The part is rated 2.5V so this does not look like a correct example. The guidance provided indicates that the junction temperature can be 125C but that is not indicated elsewhere in the datasheet. What is the maximum operating junction temperature of the CDCLVD1204? Can the device reliably operate on a 105C PCB using the power dissipation calculation example with 200MHz operation/2.5V supply? If not, is there another 1:4 LVDS buffer that will?
Was section 11 incorrectly copied from another part? It doesn't seem correct.