Part Number: CDCM6208
Other Parts Discussed in Thread: CDCI6214
Team,
is the CDCM6208 the best candidate to build a precision low frequency generator?
The device should be able to output: 50kHz, 80kHz, 100kHz, 125kHz. It doesn’t need to be precisely 50.000Hz etc. it can be slightly lower or higher as per the division will allow.
The required stability is +/- 5ppm. If not achievable, what would be achievable?
Thanks for your help.
TI Customer