This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ32000: Connecting Vback pin to the output of on LDO

Part Number: BQ32000


Hello Team , my customer has a huge Li ion battery pack in his system which he wishes to use for back up of the RTC bq32000.

The plan is to use a 3V LDO whos input comes from the Battery and the output goes into the Vback of the RTC .

DO you think its a possible idea ?