Part Number: LMK01801
Hi ,
I am using LMK01801 in my design, For the clock distribution purpose .with the following operating conditions:
Input: RF sine wave single ended
Input frequency : 2.7GHz
Clock Output 0 : 2.7GHz with output division of one.
Clock Output 4 : 1.35GHz GHz with input division of two.
Mode of controlling: PIN mode/Uwire
Based on my operating conditions ,i have initially tried with pin controlled mode with following configurations,
1.TEST/CLKOUTTYPE_0 ::High
2.SYNC0/CLKOUTTYPE_1 ::High
3.CLKUWIRE/CLKOUTDIV_1 :: High
4.DATAUWIRE/CLKOUTDIV_0 :: Low
5.EN_PIN_CTRL ::Low
With this i haven't got any clock outputs.Then i changed into uWire configuration to reflect the same still i am not getting any clock outputs.
My query is ,
1.When we are using pin control mode what should be state of uWire lines (LEUWIRE/CLKOUTDIV_2,SYNC1/CLKOUTTYPE_2) ?
2.Why there is no toggling for low frequency ,i have changed the input to 100MHz from Signal generator which is single ended ,still there is no clock outputs/Kindly clarify the same ASAP.