This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2491: lock time too long

Part Number: LMX2491

Hi,

I have built a fast stepping Synthesizer based on LMX2491 and a Crystec VCO. The frequency range is from 1640MHz to 2960MHz with 40MHz step sizes. The PLL bandwidth is around 1 MHz and the resulting lock time < 5us. So far so good.


I found a Problem at 1760MHz. At this frequency lock time is sporadically (likelihood about 10%) much longer. The PLL jumps a completely wrong frequency and stays there for exactly 100us. Someone an idea how to fix this problem?

Regards Samuel

This picture shows the voltage at the VCO (sweep from 1640MHz to 2960MHz) input with the glitch at 1760MHz.

The length of the glich is exactly 100ns