Part Number: LMK04000
Hi every one
In my design i am using LMK04000BISE PLL clock conditioner for my ADC input. The problem i am facing right now is that
the clock output (CLKOUT1 AND CLKOUT2) which is configured as output for 125MHz from reference input VCXO of 100Mhz. Instead of 125Mhz at the output i am getting offseted output of 120.05MHz which is not
even stable. But to confirm that issue i have tested with the same code configuration with another board(same design configuration) there it was working fine.
Output Clock Response:
| EXPECTED (MHz) | MEASURED (MHz) |
| 125 | 120.05 |
| 102.4 | 100.04 |