Part Number: LMK04828
Other Parts Discussed in Thread: LMX2582
Hi,
I am using PLL LMK04828 for generating 175MHz from CLKin frequency of 25 MHz with External VCXO of 100MHz. This 175MHz DCLKout has been given as input to LMX2582 PLL for generating 3500MHz.
I observed only 173MHz DCLKout at the output of LMK04828 PLL instead of 175MHz in PLL locked Status. But LMX2582 PLL is not locking with this 173MHz input.
Herewith I have attached the LMK04828 Configuration and LMX2582 Configuration file.
Kindly clarify for adjusting output frequency to out exactly 175 MHz?