This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

9DML0441 alternate device in TI

Other Parts Discussed in Thread: LMK00334

Hello,

I look for 9DML0441 alternate device. Is LMK00334 the best device for this purpose?

If yes, Is LMK00334 output driver impedance 100ohm differential?

Best regards,

Toshihiro Watanabe

  • Yes, LMK00334 is the best device.  The HCSL (current steering) driver uses an open-source output stage (high impedance).  External 50-ohm load resistors (DC-coupled) on the CLKoutX_P/N pins are required to generate the differential output voltage and to terminate the clock traces.  The driver is intended to drive a pair of 50-ohm single-ended traces or 100-ohm differential pair, since the HCSL output AC and DC specifications are given for a 50-ohm load condition in the datasheet.

    Alan