This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BAW Resonator Technology, comparison with crystal oscillators (as used in CC2652RB SimpleLink)

Other Parts Discussed in Thread: LMK05318

How does a Texas Instruments BAW oscillator compare with a typical SMD crystal oscillator for:

1) ppm stability?

2) phase noise?

3) Resistance to damage by ultrasonic cleaning processes?

4) Frequency stability, when in use, in a high-vibration environment? (e.g. in a drone, engine-management unit, avionics use etc)

  • Hi Nicholas,

    1) ppm stability?
    We are looking to target +/-50 ppm and +/-25 ppm products utilizing BAW in the near future. For CC2625RB utilizing the BAW resonator as reference, the 48 MHz frequency has a stability of +/- 40 ppm (Page 20: www.ti.com/.../cc2652rb.pdf)

    2) phase noise?
    Phase Noise performance from the BAW resonator when utilized as a VCO (example LMK05318), allows one to achieve < 50fs (@312.5 MHz) Integrated RMS Jitter (12 kHz - 20 MHz). Performance/Power tradeoff will depend on the application use case.

    3) Resistance to damage by ultrasonic cleaning processes?
    This is again a function of the how it is utilized in the application (device package and other stresses). When used as a VCO in a device like LMK05318, the loop bandwidth of the Analog PLL can be tuned to minimize the impact of vibration (25-40 kHz in the case of most ultrasonic cleaners) on the performance of the output. For CC2625RB utilizing the BAW as a reference, please post a query on the relevant E2E forum and someone from the product line will be able to better support you.

    4) Frequency stability, when in use, in a high-vibration environment? (e.g. in a drone, engine-management unit, avionics use etc)
    We have done shock and vibration testing to MIL-STD-883 standard. In general, the vibration and shock performance of the BAW resonator is superior to Quartz crystals. For information specific to CC2625RB, please post a query on the relevant E2E forum and someone from the product line will be able to better support you.

    Best Regards