Part Number: CDCE72010
Hi,
I'm trying to set up a FFMC151 Mezzanine Card from Abaco. This board contains a CDCE72010 chip and it's controlled form a FPGA.
As a first step, I just want to check that the CDCE is generating the clock signals according to the default configuration on the EEPROM, so I'm just switching the complete system on and using the output 4 of the chip as a differential clock input for toggling an LED depending on a configurable counter value (at power on, the conter value is 0). The problem is that I cannot achieve a consistent behavior: some times the clock is generated as expected and the LED blinks fine when setting a proper counter value, and some times the LED is just blinking erratically at power on. The PD pin is tied to 1 and a pushbutton is used to control the RESET pin, but even resetting the chip doesn't help.
Are there any initialization steps that I'm missing?