Other Parts Discussed in Thread: LMX2492, LMX2581
Dear Experts
I am using the LMX2592 to generate a Local Oscillator (LO) for a receiver application where phase noise and spus are important. The frequency range of the LO is approximately 4.3 to 8.3GHz with a step size of approximately one Hertz. The reference is a very low noise 2GHz source which feeds a programmable divider to bring the frequency within range of the LMX2592 OSCin. Please can you recommend input path frequencies and settings (modulator order, PFD delay, charge pump current etc.) vs output frequency to minimize phase noise and spurs?
As the output frequency range includes multiples of the reference (6 and 8GHz) integer boundary spurs are possible. Please can you suggest how to use the multiplier to avoid these integer boundary spurs? To help me understand the issues, please can you give me a good example of integer boundary spur avoidance using the multiplier on the evaluation board?
Thanks in anticipation.
John