Part Number: CDCLVD1208
Other Parts Discussed in Thread: LMK04808
The input specs of the buffer show a differential input range of 0.3V – 1.6V. But the output specs of the buffer show the differential output magnitude to be from 250mV to 450mV. Does this mean that the differential output of this buffer could potentially not be within the input specs of itself?
I have a customer that plans to daisy chain these buffers together. Is this possible given the specs?
Thanks.