Part Number: CDCM7005-SP
Hi,
Can you please provide a lead forming for using the above part?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCM7005-SP
Hi,
Can you please provide a lead forming for using the above part?
Thank you.
Hi,
Thanks for the reply.
1. however, the dimension "M" in the fancort footprint, which shows the dimension of the chip is given 0.758".
this is different from the datasheet which indicate only 0.542~0.558".
Quad_Pack_Spec_Sheet_4208539.pdf
2. Can i have the IC thickness? it seems to be missing from the mechanical data of the chip.
Hi,
It seems Fancort has not published the updated version which I have attached here showing the correct dimensions. Also, the end of the datasheet provides more detail on dimension "C" just below the the graphic you have provided (see below).
If this provides answers to your questions, please check the appropriate box.
Thanks
Christian