Part Number: CDCLVP111-SP
Can you help with the below question regarding the LVPECL clock driver CDCLVP111-SP.
I wanted to see if I could get some clarification for input threshold for the device. On Pg. 7 of the datasheet the minimum input amplitude is specified as 0.5V. From what I could gather on TI support questions(http://e2e.ti.com/support/clock-and-timing/f/48/p/761088/2813337#2813337?jktype=e2e) it looks like this is referring to the single ended input the device sees. Is this correct? So when looking at the differential signal the thresholds will be +/- 500mV. Is that a correct statement? Thanks.