Hello
I have a particular board that is showing the phase difference after the R divider and N divider is bigger than other cards for PLL1. We are using the STATUS pins and an oscope to see what the signals look like after the dividers. This means that we have to increase the window size in order to see the lock LED light up. This doesnt make much sence as it should be the same for all cards.
I have replaced every component in the loop filter and nothing changed. Since the loop is internal to the LMK0426, is this a normal thing where sometimes there is a phase difference between parts? Our other cards will show that the signals are aligned within 4nsec, but on this card its like 9ns.
Please assist. I didnt find anything in the datasheet that mentions part variations between lots. I am thinking of replacing the LMK0426 just to see if it changes.
Thanks
Layne