Part Number: LMK04828BEVM
Tool/software: WEBENCH® Design Tools
have a similar issue using the 128MHz output from a LMK04828BEVM to be the CLKIN1* input to a 2nd LMK04828BEVM in order to generate two LVDS outputs at frequencies 350MHz and 490MHz. Should I also use the on-board 122.88MHz oscillator so as to have the PLLs form a stable closure? The clock design tool doesn’t clearly show the use of this input as there is only one input clock in the upper left of the GUI window.
Attached is my setup using the clock design tool that won't lock either PLL. I've tried suing the linked Webbench Clock architect tool with the NSC Clock design Tool and can't get the two to agree. The Webbench tool doesn't give me the PLL1 R and N dividers or the PLL 2 R, N, and N Pre dividers that are need to be set in the TICS Pro tool.
LMK04828-dual-loop, 128 MHz to 122.88 MHz to 2450 MHz to 350 MHz and 490 MHz.txt