This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: t1, t2 delay

Part Number: LMX2594


Hello team,

I have a question about phase synchronization.

Datahseet figure24 shows a concept of the function, and t1 and t2 delay is mentioned in the figure.

Does both t1 and t2 delay time have dependency on Fosc?

In other words, does LMX2594 shows different t1 and t2 delay time when comparing Fosc=40MHz case and Fosc=50MHz case with exactly same register settings?

There is a description that the delay time is dominated by VCO calibration time. If Fosc changes, state machine clock frequency also changes, so I think LMX2594 shows different t1 and t2 delay time if changing Fosc frequency. Is it correct?

Best regards,