Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594, LMX2595
Hi,
I have questions regarding register values for register 0 and 25 in the LMX2594 and wonder if you can help?
In register 0, D3 is responsible for FCAL_EN, should this be toggled (0 - 1 - 0) if so how long should it be high for, or can it be left as 1?
Regarding register 25, revision B of the data sheet shows that D11 = 0, D9 = 1, D3 = 0, D2 = 1, D1 = 0 and D0 = 1 - these appear to be fixed values and not responsible for any user defined functions. However, if I download the hex file from the evaluation board using TICS Pro all of these values are inverted. Which of these settings are correct?
I ask because we have problems with very high phase noise and wonder if one of these register settings could be a contributing factor?
Many thanks for any help you can offer,
Best regards
Keith