Part Number: TPL5010
Other Parts Discussed in Thread: TPL5000
Hello E2E,
I am looking to use the TPL5010 (or one of its sister devices) in a power reset application. At a high level, when a power disable function is asserted, I need to assert for 5s. Then, after ~30sec, I need to assert another signal to turn my device back on. I plan on using 2 x tplxxxx devices for this. However, it appears that upon startup, there is always a pulse. Is there a flavor of these nano-timers that does not do this? Is there a workaround for these kind of situations?
Thanks!
Russell