Part Number: LMX2594EVM
Hi !
I'm making some measurement about the lock detect timing using the Full assist mode, and I cannot explain one phenomenon:
- First, I have used the interface in order to program the different parameters for the Full Assist mode. From the frequence F1 to F2, I measured around 20µs between the rising edge of the CSB and the rising edge of the Lock Detect
- Secondly, I decided to directly load all the registers corresponding to the frequence F2. To do that, when the PLL was locked on the F1 frequence, I programmed the current charge pump to 0mA, and the I loaded all the register. The lock detect was activated immediatly after the rising edge of the CSB linked to the R14 (as expected) but this time, I measured a time around 5µs.
So I would like to know if that behavior is normal or not ?
Thanks
Stéphane