I've use BQ4802Y as system real time clock. VCC is 5VDC, VBC=3VDC Li Battery. I set the /STOP=1 in control register(E) and ABE=1 in Alarm enable register(C). I've checked that Control Register(E) content=06h, Flags Register(D) content= 01h, Alarm enable Register(C) Content=09h. when power by VCC the BQ4802Y is working correctly but when power by VBC clock is not keep clocking. So when BQ4802Y be power by VCC again, the clock is start to clock from at VCC off. I use VOUT to power SRAM and found that SRAM content are retained correctly. I don't known what's wrong about above mentioned problems ? I already try couple of weeks on this problem. I hope someone can help me to solve it. Kind regards; Marshall Wu 2019/04/14